Micronas presents the robust direct angle sensor family HAL 37xy offering outstanding temperature stability, high resistance against air gap variations and magnet aging together with a wide-range of diagnostic functions and very effective protection circuitry.
Micronas announced today that Günter Hoppe, the CFO of Micronas, will retire as planned as at November 1, 2014. His successor, Daniel Wäger, will take office until November 1, 2014.
With the HAL 15xy, Micronas introduces the successor of the HAL 5xy family, which is well-known for a long time on the market for excellent quality and highest reliability, proven by a large installed customer base worldwide and widely used today in all premium car brands.
Micronas Group's consolidated net sales went up in the first quarter of 2014 by 7.4 percent to CHF 40.2 million despite the continuing weakness of the yen. The Automotive segment saw sales improve on Q4 2013 by 4.9 percent to CHF 37.3 million, while the Industrial segment posted sales growth of 54.7 percent to CHF 2.9 million.
The new USB kit for user-friendly and flexible programming of various Hall-effect sensor families from Micronas was designed especially for use in the development laboratory and offers an efficient, easy to handle, and affordable solution.
HAL 1002 from Micronas is specifically designed for use in automotive and high-end industrial applications, demanding high programming accuracy under harsh environmental conditions up to a 150°C ambient temperature.
Micronas performed well in a demanding market environment in 2013. Despite the persistent weakness of the yen and continuing volatility in the car industry, the Company was able to strengthen its leading position in the market for Hall sensors used in automotive electronics.
Micronas paves the way towards a new class of highly versatile, single- chip smart actuator solutions by licensing a high-performance 32-bit core for their HVC family
By the installation of a combined heat and power (CHP) unit, Micronas trusts in alternative energy generation, and at the same time, reduces its operational costs. This investment is another clear commitment to the production site Freiburg.
The Career Fair on campus of the University Furtwangen offers twice a year students and graduates the opportunity to make personal contacts with companies - for example with Micronas who must not be missing.
The Automotive Suppliers' Day Baden-Wuerttemberg is an established meeting place for many years in the automotive branche. The event will take place on 12 November 2013 at the Haus der Wirtschaft in Stuttgart.
Micronas Group’s consolidated net sales increased to CHF 39.0 million in the third quarter of 2013. For the first nine months of 2013 the Company achieved sales of CHF 114.5 million, compared with CHF 130.3 million for the equivalent period of 2012. The main reason for this decline is the continuing weakness of the Japanese yen.
Following the successful launch of its HAL 24xy sensor family with HAL 2420 and HAL 2425 derivatives, Micronas now presents the HAL 2455 with PWM output and makes available all derivatives in SMD packages
"Thanks to consistent implementation of product quality standards, close collaboration with our customers and continuous innovation, Micronas is in a leading global position," says Matthias Bopp, CEO of Micronas.
With the TO92UP package, Micronas has developed an AEC-Q100 qualified leaded package with a surface of only 29 mm2 and thus offers a new attractive package for its Hall-effect sensors
With the HAL® 83x family Micronas enlarges its portfolio of the successful Linear Hall-effect sensors HAL 8xy and offers a solution especially tailored for the detection of low magnetic field strengths together with increased measurement accuracy and improved ESD protection.
Micronas saw its positive performance continue in the 2012 financial year, with sales and earnings both up on 2011, especially in the Automotive division.
The first derivatives HAL 2420 and HAL 2425 of the HAL 24xy sensor family allow the measurement of larger distances with smaller magnets, providing substantial cost benefits when used in sophisticated and demanding automotive and industrial applications.