Trade News |

New Family of Hall-Effect Sensors from Micronas Integrates Microcontroller and Digital Interfaces (0803)

TDK Micronas Visual

Freiburg, Germany – February 14, 2008 – Micronas (SWX Swiss Exchange: MASN), a leading supplier of innovative application-specific IC system solutions for automotive and consumer electronics, today announced the HAL 28xy series, a family of Hall-effect sensors optimized for automotive and mechatronic applications that demand accuracy and flexibility combined with low cost. The HAL 28xy is the first Hall-effect sensor family to include a microcontroller, a temperature sensor, advanced on-chip compensation, and a digital interface.

The latest automotive designs require smart sensors to deliver the high level of precision and robustness linked with the capability of local pre-processing of the measured data. HAL 28xy devices meet these needs with a programmable on-chip microcontroller that makes each device more adaptable and more accurate and provides diagnostics for additional reliability and ease of service. The digital interface reduces component and wiring costs, making HAL 28xy family members cost-effective for applications such as seat-track position and fuel-level sensing.

“The HAL 28xy family is highly flexible, offering a fast implementation scenario for new output formats. With the built-in RISC processor we are even able to offer customer-specific signal processing.” says Peter Zimmermann, Market Manager Automotive at Micronas. “This flexibility allows OEMs to save time and money in the development cycle.”

The key to overall accuracy are three types of error correction. The Hall-effect sensor and on-chip temperature sensor each have their own analog-to-digital converter (ADC). This lets the microcontroller perform spinning-current offset compensation, plus first-order temperature compensation for Hall offset error and second-order temperature compensation for overall Hall-effect sensitivity. The on-chip EEPROM makes it possible to store custom individualized application parameters in each device.

The implemented bus interface can drive the serial bus directly because the bus-driver is fully integrated. Both the power supply and the serial bus connections are protected by over-voltage devices. Family members include devices with LIN bus, used for most interior and passenger comfort applications, SENT, targeted for engine management, and PWM, addressing power steering applications.

Along with the HAL 28xy, Micronas offers an easy-to-use application kit containing a programmer board, LabVIEW™ programming software and the necessary source code. Key application variables such as sample rate, magnetic field range, sensitivity, offset, and the temperature coefficients of sensitivity and offset can be adjusted by programming the non-volatile memory. Programming is done via LIN frames or BiPhase-M telegrams, depending on the family member.

All HAL 28xy family members are offered in a TO-92UT package rated for use from -40 to +140°C. Pricing and availability vary with model.